STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9565 Views
  • 5 replies
  • 3 kudos

debug the TMC5130 eval board

helloi am working with the TMC5130 eval kit. its a motor control driver that is controlled by STM32f205 chip.the IDE is based on eclipse IDE, and for now all i can do is build my project (there are few build configuration files) and program it via US...

Aasaf.1 by Associate
  • 1645 Views
  • 1 replies
  • 0 kudos

Resolved! Count rotation circles during motor rotation

Hy dear helpers,I am using STM32G431CB, I generated code with the help of motor control workbench. Everything works fine, but I can not count how many circles the motor rotated. I would like to do the following: Start the motor, do 5 whole circles, t...

N_1 by Associate II
  • 2070 Views
  • 3 replies
  • 0 kudos

bldc motor control using nucleof429zi

Hi, I'm trying to drive bldc motors for multicopter. So I sent PWM signal to esc using timer on my board. It works on SimonK firmware but BLheli does not work. I want to use BLheli firmware... How can I fix it? I think its protocol is Oneshot42

Jbaek.1 by Associate
  • 1514 Views
  • 3 replies
  • 0 kudos

Running a BLDC motor through STM32CubeIDE commands

I have a P-Nucleo-IHM03 motor control pack, that includes a G431RB MCU, IHM16M1 driver board, and GBM2804H-100T BLDC motor. I am trying to simply create a project in the STM32CubeIDE that makes the motor turn. I went through the process of creating t...

MSzos.1 by Associate II
  • 1340 Views
  • 2 replies
  • 0 kudos

How to control a keyestudio 9G servo motor (2 commands)?

Hello,Actually I want to control a keyestudio 9G servo motor, the problem is that when I send 2 commands to turn it right it turns for the first call and gets stuck for the second one, yet when it comes to the documentation,It says it's a 90 degree m...

OFati.1 by Associate II
  • 1265 Views
  • 2 replies
  • 0 kudos

STEVAL-CTM010V1 board can not work

I've just got CTM010V1 board at hand, after powering on with 220VAC input:there's is no led lit up after powering on demo board"ST motor control workbench" seems no connection with CTM010V1 to PC via RS232 USB cableCould anyone help me to get start w...

JerryL by Associate
  • 2104 Views
  • 2 replies
  • 0 kudos