cancel
Showing results for 
Search instead for 
Did you mean: 

Can STM32G4 control 4 bldc motors?

QuirinS
Associate III

Hello i want to build a drone esc. So I need to control 4 bldc motors with a mcu. How would i do this? In the MC Workbench i can only select 2 Motors max.

1 REPLY 1
GMA
ST Employee

Hello @QuirinS,

Referring to this post, B-G431-ESC board could be a solution.
It’s possible to control the B-G431-ESC board from a PWM input to vary the speed with the Electronic Speed ​​Control. You can, for example, have 4 B-G431-ESC boards and one central control board.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA