STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9565 Views
  • 5 replies
  • 3 kudos

Resolved! STEVAL-SPIN3201 SWD Programming

STEVAL-SPIN3201After looking at the schematic i can see that there is a second MCU to 'control' the STSPIN32F0. This second MCU has a STLINK connector for programming. My question is ; Is it possible to program the STSPIN32F0 directly and not have to...

PKAci.1 by Associate II
  • 1695 Views
  • 2 replies
  • 0 kudos

Resolved! problem with SPI daisy chain

Hello,I am using IHM02A1 expansion board (on top of L073RZ), which has two L6470 connected in a daisy chain configuration. I cannot receive any data from the devices. What do you think the reason can be ?Below is the bus status of a reset and get par...

0693W000006FZgkQAG.png
mete by Senior II
  • 4071 Views
  • 6 replies
  • 0 kudos

B-G431B-ESC1 has issues powering a BLDC pump application

I have a BLDC fuel lift pump that I would like to power using the B-G431B-ESC1 board.I have gone through the issues as described with the Y version of the µC, and can test the system using the motor profiler.This program is able to spin up my device ...

GStou by Associate III
  • 1078 Views
  • 1 replies
  • 0 kudos

Resolved! B-G431B-ESC1 MotorControl "wrong" current measurement (how to obtain the average current through the windings)

Hi ST CommunityI am using a default MotorControl setup with the B-G431B-ESC1 board and a BLDC motor with hall sensors. The project is generated using MC Workbench with default values. I am having a hard time to decipher the value provided by the func...

JA.1 by Associate III
  • 5057 Views
  • 8 replies
  • 0 kudos

Resolved! STSW-SPIN3204 firmware questions

Hello Friends and ST engineer.I am controlling BLDC motor using STSW-SPIN3204 firmware with Hall Sensor. But some functions I do not understand, please explain more detail for me.HAL_TIM_OC_DelayElapsedCallback: what is this function for? why we use ...

Vnguy.1 by Associate II
  • 4221 Views
  • 9 replies
  • 0 kudos

Brake the motor in FOC?

Is there anyone here could show me how to find the break function or instruct me how to apply break the motor please? I'm using G431B ESC1. As from the Release Notes for X-Cube-MCSDK, there are couple of ways to use break in FOC: Dissipative DC link ...

PPhan.1 by Associate II
  • 1907 Views
  • 1 replies
  • 0 kudos

MCU facing some problem,

Dear STM team, Here we have using STM32f405RG MCU, for the e-bike motor controller applications. The programmer is STLink v3. Now we face some stuck in the stage, what happens in the IDE, once am using debug mode it's going to hold in stack point pla...

0693W000006FOK4QAO.jpg

Preferred motor control method

Hi everyone,I have a hobbyist drone motor with the following phase voltage plot. Can anyone recommend the preferred method of controlling this motor? Is (sensored) trapezoidal or sinusoidal control sufficient? Or do we have to use FOC control?Thank y...

KZhan.6 by Associate
  • 1941 Views
  • 2 replies
  • 0 kudos