STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

Resolved! CubeMx "can't add: motorcontrol files not found" problem

Hi everybody.When i open "SDK5x - STEVAL-SPIN3201 - BullRunning.ioc" file (that is pre-compiled example FOC motor control firmware provided by ST), "can't add: motorcontrol files not found" fault message appears on my screen. I already copied Motor C...

Ebuko.1 by Associate
  • 4211 Views
  • 4 replies
  • 0 kudos

Dual drive with FOC with STM32G431

Hi,for a project I would like to design a dual BLDC drive based on STM32G4 microcontrollers with FOC algorithm for both BLDC motors.In a first view STM32G431 with 64 pins and two STSPIN830 and 3 shunt current measurement seem to fulfill the project r...

JKoch.1 by Associate
  • 1758 Views
  • 1 replies
  • 2 kudos

Low Speed Hall Sensor

Hi,I have been struggling to run my motor at low speeds and I suspect the Hall Sensors are the limiting factor. In UM1052 I found the following line on page 36. "For speed regulation, there is absolutely no need to have a sampling time lower than the...

nmamore by Associate II
  • 1924 Views
  • 1 replies
  • 0 kudos

Can a single STM32G4 be used to (sinusoidally) control 6 high-current BLDC motors, each with 3 digital Hall effect sensors, and each using 3x PWM Mode for control?

We would like to use an STM32G4 to (sinusoidally) control 6 high-current BLDC motors, each with 3 digital Hall effect sensors, and each using 3x PWM Mode for control (in addition to monitoring the voltage across 1 or 3 shunt resistors on each motor f...

Ricardo1 by Associate II
  • 1261 Views
  • 1 replies
  • 0 kudos