STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1734 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9578 Views
  • 5 replies
  • 3 kudos

STEVAL-PCC009v2 SDK bug

Posted on March 21, 2012 at 16:45Hello all, I tried to use the USB to serial interface SDK for the STEVAL-PCC009v2 dev board to write a custom driver for the L6470 (EVAL6470 board). The included library SPI_SDK.dll works fine, but the command: DFU_G...

Where is PMSM SDK V3.2?

Posted on July 04, 2012 at 08:04I can't find the PMSM SDK V3.2 but it referred in UM1052 : STM32F103xx/ STM32F100xx/STM32F2xx/STM32F4xx PMSM single/dual FOC SDK v3.2

reza1199 by Associate
  • 1549 Views
  • 3 replies
  • 0 kudos

Motor control with steval IFN003v1

Posted on September 06, 2012 at 15:37Hi, I work on motor control with  : ''STEVAL IFN003V1''. I've generate a file (.h) with all parameters with ''ST MOTOR CONTROL WORKBENCH''. But it's my first utilisation of library ''foc sdk 3.2'' Could you show ...

undefined reference to `MCboot'

Posted on September 12, 2012 at 15:59Hi, I work on atollic with stm32 foc sdk 3.2 for motor control. When I compil my project, I have always the same errors : ..\srcmain.c:40: undefined reference to `MCboot' ..\src/main.c:41: undefined reference to...

Problems with SDK3.2 and MCWB 2.0

Posted on September 14, 2012 at 02:21I have an IPMM with absolute position resolver mounted on it. Unfortunately i can not use it even with decoder - absolute position to 12-16 bit paralel interface. Thats why i try to run in sensorless modes with 2...

FOC SDK V3.2 confidential distribution

Posted on October 02, 2012 at 11:51I have changed FOC SDK V3.0 to work with a linear motor with analog hall sensor and these changes work so far with the STM32F103RC microcontroller. But actually I have planned to use STM32F205RB microcontroller for...

fortunat by Associate II
  • 1471 Views
  • 3 replies
  • 0 kudos

3Phase Induction Motor with FOC SDK3.2

Posted on November 04, 2012 at 11:19Hello... I do want to have motion contol with 3Phase induction motor with FOC algorithm. The FOC library(FOC SDK v3.2--UM1052) and software(ST Motor Control WorkBench) offered ST is for PMSM. I dont want to use Pe...

saraaj100 by Associate II
  • 4489 Views
  • 9 replies
  • 0 kudos

Has STM32 MC FOC SDK V3.3 released?

Posted on December 13, 2012 at 00:37Hi, I noticed that  STM32 MC FOC SDK V3.3 was mentioned in ST Motor Control Workbench V2.1 as one of the target libraries. I also found a http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REL...

tamil by Associate II
  • 1575 Views
  • 3 replies
  • 0 kudos

IHM023V2: FOC duration fault

Posted on February 07, 2013 at 14:11Hardware: STEVAL-IHM023V2 + STM32100B-EVAL + custom motor Configuration: High-voltage 3-phase PMSM, IAR 6.50.2.4585, STM32 PMSM FOC Firmware Library v3.2 - WEB distribution I'm trying to get started with the examp...