STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9587 Views
  • 5 replies
  • 3 kudos

Resolved! AC Servo motor solution

Hi all,Does ST have any solution for Development of Driver circuit of "Permanent magnet synchronous AC servo motor" and "AC induction servo motor".

sanju by Senior
  • 1426 Views
  • 2 replies
  • 0 kudos

Resolved! Do X-CUBE-MCSDK will support AC induction motors?

Posted on June 17, 2018 at 12:25Hello,For the moment, X-CUBE-MCSDK only support PMSMs and BLDC motors.However, AC inductions motors are not supported yet, that's a shame because this kind of motor is still very present in the majority of industrial ...

Resolved! Sampling 3 phase current with only 1 ADC

Hello,In motor control pack P-NUCLEO-IHM001, microcontroller is STM32F302R8 which has only 1 ADC.The motor drive has option to use 3 current shunts.By analyzing the datasheet, ADC does not have multiple sample & hold circuits.So, how would it be poss...

MMila.3 by Associate
  • 1492 Views
  • 3 replies
  • 0 kudos

Cannot build generated code

After generating the project with Motor Control workbench and building it on CubeIDE, I get this error : 15:10:13 **** Incremental Build of configuration Release for project Noname ****make -j4 all arm-none-eabi-gcc "../Src/aspep.c" -mcpu=cortex-m4 -...

Rced.1 by Associate
  • 1581 Views
  • 3 replies
  • 0 kudos