2016-06-21 8:49 PM
Hello,
What I have done so far is ....1. parameter setting using Motor Profiler2. Can control motor speed (Main sensor is Hall sensor. Aux sensor is observer +cordic)But my problems and questions are ... 1) Even using Hall sensor, Ramp up procedure is needed ?2) When change direction, I do like this.. - ramp-up to 300rpm (ccw) - speed up (ccw) and rolling.... - speed down (ccw) to 300rpm - motor stop command when speed is under 300rpm - ramp-up to -300rpm (cw) - speed up (cw) and rolling... but the problem is every time motor should stop. So motion is not good. not smooth. How can I control smoothly?Thank you very much in advance.2021-06-27 10:06 PM
Adding of STM32 Motor Control topic.
Best regards.