STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9587 Views
  • 5 replies
  • 3 kudos

Resolved! Soft Starter for 3 Phase Induction motor

Posted on April 05, 2017 at 09:14Hii all,I am doing project on soft starter of 3 phase Induction Motor using Stator Voltage control method. Has anyone done program for that??Please give reply as soon as possible.

Why does the CCR value not Updated?

Hi All,I would appreciate your help with this problem.I am presently trying to implement the PWM scheme PWMON as shown in figure below.I have set the polarity of the timer's main and complementary output to be LOW. And it runs on PWM Mode1.And then a...

0693W000008xZwfQAE.png 0693W00000BajEyQAJ.png 0693W00000BajJsQAJ.png

Speed Control of 3-Phase Induction Motor

I'm designing project for Speed Control of 3-Phase Induction Motor with STGIPS30C60-H. I'm driving with microcontroler trough optocoupler. The motor is rotating in with desired speed about one minute and after stop. After that STGIPS30C60-H does not ...

MTole by Associate II
  • 1313 Views
  • 1 replies
  • 1 kudos