STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

STM3210E-EVAL motor control example

Posted on January 18, 2012 at 17:00Hi, I'm trying to get a motor control example running on the mentioned board - without success. My main function looks like this: int main(void) {   SystemInit();   Demo_Init();   //initialize motor control lib  ...

Stimulate error on motor

I use Lib version 4.3 to control SM-PMSM.The motor can run smoothly.However I would like to simulate 2 error hereafter.SW error (FOC Frequncy cannot be sustainable)Start up fail.I would like to check these 2 error without modify code. PS.I have lock...

JRoja.16 by Associate
  • 959 Views
  • 1 replies
  • 0 kudos

Motor start vibration problem

I use FOC+Hall sensor(STM32F030RE MCU, ihm08m1 power board, MC lib 5.3.2).I try to start motor using MC_ProgramSpeedRampMotor1() function, but the e-bike has "start vibration" problem.How to avoid this problem? adjust pid or something else?any sugges...

cyt by Associate II
  • 1240 Views
  • 1 replies
  • 0 kudos

Question for Motor Control Firmware FOC V2.0

Posted on January 22, 2014 at 23:51Hello, Does anyone know where I can find the Source Files for the ''MC_FOC_Methods_lib.lib'' and ''MC_State_Observer_lib.lib''?There are parts of the open source code in the library files, where you can not look in...

hans by Associate
  • 1743 Views
  • 4 replies
  • 0 kudos

Absolute Encoder for St Motor Control library

Dear,I know that ST Motor control library does not support Absolute encoder, so I am trying with some difficulties to do it, I connected my motor with HALL sensor and also connected my absolute encoder with SPI, I can read the abs position without an...

JEsca.1 by Associate II
  • 2372 Views
  • 3 replies
  • 0 kudos