2017-06-11 7:29 PM
The motor profiler starts profiling starts to measure the motor parameters like R,L ,Kb and other mechanical parameters but every time i use the values are different from physical measurements which gives me a confusion when to rely on Motor profiler and when not ?
I want to understand the Algorithm so that i can know where to use values measured by profiler and when to mesure using test setup.
#stm32-foc-pmsm-sdkv3.0 #inductance #motor-profiler2021-06-27 10:02 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.