STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

ASPEP - how is synchronisation done ?

Hello thereI´ve consulted documents explaining the ASPEP - I´m still wondering how synchronisation is done. -Like is there a unique token / value / ASCII character marking the start or end of a telegram?E.g. the NMEA protocol for GPS antennas use the...

Humming Noise at High RPM Using Sensorless FOC

Hi Everyone,We are using an STM32F401RE Nucleo board with the IHM16M1 power board, running a sensorless FOC algorithm generated using ST Motor Control Workbench. The motor parameters were averaged over several runs using ST Motor Profiler, and the co...

speed.PNG
Mani2 by Associate III
  • 1856 Views
  • 10 replies
  • 0 kudos

Iq and Id PID oscillating/unstable after some time

Hello,we do have a custom motor control board based upon B-G431B-ESC1.A custom inverter board is created with the board designer and the project is created with MotorControl Workbench 6.3.1. The system is running fine at higher RPMs (>2500 RPM; max R...

CWern.1 by Associate II
  • 2831 Views
  • 7 replies
  • 1 kudos

ASPEP -> add own commands / endpoints?

Hello there-Is there a way to add own commands/requests to the ASPEP protocol like retrieving own custom introduced values?I´m running the B-G431B-ESC1 board and adapted the esc.c file to my needs and it now holds a value I´d like to be able to retri...

MCSDK 6.41 with Custom board - internal opamp

 Subject: PMSM Motor Drawing Higher Power at Low RPM – Guidance on Parameter TuningHello Expert,I have developed a custom board based with STM32F303VET6X, using two IPMs and 0.47 Ω shunt resistors, similar to the STEVAL-IHM045V1 design. The board uti...

stspin32g4 EMI radiated issue

"Hello.We are currently developing a medical device in Korea using the STSPIN32G4.During an EMI pre-scan, we confirmed that noise is being generated in the 188MHz band from within the chip.We have seen posts on forums from others who are experiencing...

Crazyoh_0-1761787604471.png Crazyoh_1-1761787686476.png
Crazyoh by Associate
  • 401 Views
  • 2 replies
  • 0 kudos