STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1816 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4956 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9713 Views
  • 5 replies
  • 3 kudos

MCSDK / FOC SDK for STM32F2

Hello, I have read that the support for STM32F2 in FOC SDK / MCSDK is skipped after 4.x. Is that right, if so, where can I get the latest 4.x version for my STM32F2 design? Thanks in advanced

MiJes by Associate II
  • 1491 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 Motor Control - STM32G474xx - HRTIM Support?

Hello,Are there any future plans to add HRTIM Support in ST Motor Contol Workbench? As far as i have seen G474 is inculded, but only with TIM1 and TIM8. Though these two are the advanced motor control timers, i need a faster PWM signal for my applica...

GPoll.1 by Associate
  • 2776 Views
  • 2 replies
  • 0 kudos

B-G431B-ESC1 is bidirectional?

I intend to drive a BLDC with regenerative braking. i would like to know if the B-G431B-ESC1 component works bidirectionality, since during the regenerative braking there will be current return. I will also integrade a Buck/Boost DC-DC bidirectional ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.