STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

Resolved! MCSDK 6 STMCWB won't start

Hello.I'm trying to use MCSDK for EVLSPIN32G4-ACT demo board on Win7_x64 PC.After installing X-CUBE-MCSDK-FUL_6.2.1, MotorControl Workbench do not start at all.STMCWB.exe exits after splash screen without any notice,STMCWB_C.exe prints such error:......

Resolved! ST Evaluation Board EVSPIN32G4

Hi   i have recently purchased for ST Evaluation Board EVSPIN32G4   Supply voltage Nominal From 10 V to 75 VMaximum output current with heatsink (EVSPIN32G4) Peak 35 AContinuous(1)  20 Arms Maximum output current without heatsink (EVSPIN32G4NH) Peak ...

Resolved! MCSDK inverter

I'm using mcsdk and want to create an inverter file based on STM32G070CBTx, but when generating the project, it tells me that my selected hardware is not compatible with the algorithm

iskan by Associate III
  • 3818 Views
  • 7 replies
  • 0 kudos

ST Evaluation Board EVSPIN32G4

Motor Control Workbench 6.2.1 I Have using the above version Pilot software. i am getting Speed feedback Err in BLDC Motor application. before i was try Hall Sensor Position Sequence value find and fill it . but i can't solve this fault.  any one sup...

Six step BLDC Control(X-NUCLEO-IHM11M1)

Hi,We have been using the X-NUCLEO-IHM11M1 driver to drive a BLDC motor. We were trying to read encoder values from the motor. The driver experienced short circuits on two occasions despite receiving sufficient voltage i.e. 3.5V to operate the BLDC m...

_Danny_ by Associate III
  • 675 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G4 BLDC HALL SENSOR

Hi,I am making a project using stm32cubeide for BLDC motor with Hall sensor.First project generated using timer2 made for Hall sensor reading with Combined Channel XOR ON / Hall Sensor Mode option, motor is working correctly, interrupting reading Hal...

kulfi27 by Associate II
  • 7080 Views
  • 4 replies
  • 1 kudos