Hello,
I bought two EVLSPIN32G4-ACT motor control evaluation boards and tried to setup CAN-FD communication between them.
Then I came to know it doesn't have a CAN transceiver IC(U3) populated on board. Image attached for your reference.
Can an...
Hi @Curve Wrecker Check again with all the parameters like board and motor selection initially. Also make sure you are using updated version of the software(MC Workbench, Cube MX, IDE).Try resetting the board if no response(after flashing the code).
Hi @AShah.14 Thanks for considering it.There is not any option given to modify the composite condition in MC Workbench. Also gone through the documentation, there's not much supported information regarding this problem.If there's is any alternate so...