STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1808 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4951 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9703 Views
  • 5 replies
  • 3 kudos

SENSORLESS MOTOR CONTROL TUNING

hello community,I am using IHM17m1 with nucleo F401RE to control an 3v bldc motor from maxon , facing some issues in tuning issues------------------------------------------------------------------------------------------------------------------------...

hashiR_0-1727075914594.png hashiR_1-1727076092046.png hashiR_2-1727076423495.png
hashiR by Associate III
  • 2295 Views
  • 5 replies
  • 2 kudos

torque control issue in bldc motor control

hello everyone ,i am working with ihm17m1 for driving an 3v bldc motor in sensorless algorithm , facing some issues with speed control mode issue1 - even after changing the motor parameters according to my motor , its showing speed feedback error aft...

hashiR by Associate III
  • 1083 Views
  • 0 replies
  • 0 kudos

speed and torque control in motor control workbench

hello everyone ,i am working with ihm17m1 for driving an 3v bldc motor in sensorless algorithm , facing some issues with speed control mode issue1 - even after changing the motor parameters according to my motor , its showing speed feedback error aft...

hashiR_0-1727081975196.png
hashiR by Associate III
  • 849 Views
  • 0 replies
  • 0 kudos

Motor Control problem in positioning

Hello community, i have a problem with Motor in Position mode.I use kit of two boards X-NUCLEO-IHM08M1 and NUCLEO-G431RB. I connected quadrature encoder using ABZ interface. Everything works well when motor rotates in diapazon from -180 rad to +180 r...

ABask.1 by Associate II
  • 5363 Views
  • 6 replies
  • 0 kudos

STM32 and L9907 integration support

Hi,I have a custom motor control  board with STM32F302R8T6 as controller and L9907 as the driver. Could you suggest any example codes I can use for the integration? I could not find anything available in Motor control work bench and AutoDevKit Studio...

BalaB13 by Associate
  • 2137 Views
  • 3 replies
  • 0 kudos

Significant IqREF jumps while motor running

We're having following issue with our motor control:The motor is running fine, however one can hear irregular "hickups" in the regulated speed.We did some tracing and found that the IqREF value has a significant jump up (~20A) and then back down afte...

MotorPilot_7pWcBc4bui.png
DMeie.2 by Senior II
  • 3602 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.