STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Imax Setting for 2928.86 gf·cm Torque Operation

I would like to ask for your guidance regarding the motor current setting under a specific torque condition.Based on the motor datasheet,I derived a linear torque–speed relationship and confirmed that, at a torque of 2928.86 gf·cm,the motor is expect...

pelino_0-1770472140317.png pelino_1-1770472194019.png pelino_2-1770472744539.png
pelino by Associate III
  • 233 Views
  • 1 replies
  • 0 kudos

Motor startup in sensored mode

Hi everyone[PN]: STM32F303RE, X-Nucleo IHM17M1, Faulhaber 0620-006B[VERSION]: 6.4.1[TOOL]: MC Workbench setup[DETAILS]: Hi everyone. I'm currently trying to configure the aforementioned hardware for motor control. My question is in regard with sensor...

Is it possible to calibrate Steval-esc001v1?

Hi,I am working in steval-esc001v1. I have set the a2212-13t-1000kv bldc motor to ran at minimum of 1000 rpm and at maximum of 9924 rpm using the foc algorithm in the motor control workbench software. I have ran till the 8000 rpm. But our goal is to ...