STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX Audio Class frame done callback not called

I've set up my STM32U5A9J-DK to use ThreadX and connect to my PC via USBX and Audio Class.I'm correctly see the Audio Device on my PC and I can easily stream audio to it. The only thing is that, for some reason, the callback for new frame done is not...

nico23 by Senior III
  • 2569 Views
  • 21 replies
  • 3 kudos

Resolved! VENC_SDCard_ThreadX Example

Hi, @krastThe readme for the VENC_SDCard_ThreadX examplehttps://github.com/STMicroelectronics/STM32CubeN6/blob/main/Projects/STM32N6570-DK/Applications/VENC/VENC_SDCard_ThreadX/README.mdstates:"The output is raw since no file system is used for now"b...

Resolved! STM32F407VET6 Black Pill V2

I procured an STM32F4VE 2.0 board *Details of board here:*https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0I managed to create a Basic STM32 Cube Project for this controller. (STM32F407VET6)From the Schematic on STM32base website, I see PA1...

nagendra_1-1764608023780.png nagendra_2-1764608076266.png nagendra_4-1764608204186.png nagendra_0-1764607947951.png
nagendra by Associate
  • 824 Views
  • 2 replies
  • 1 kudos

Resolved! Error in PSSI HAL code for HAL_PSSI_Abort_DMA

I am working with an STM32U575, HAL version 1.5 and found the issue described below(Have checked the HAL code for the H5 and H7 and these contain the same issue)See picture below, when aborting an PSSI transfer, before checking the state on lines 125...

LVan31_0-1718625311115.png
LVan .31 by Associate III
  • 1725 Views
  • 3 replies
  • 1 kudos