STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I am trying to communicate Uart in interrupt mode.We are able to successfully transmit & receive data to PC (through USB-UART).But when we connect to UART based modem then we are getting HAL_UART_ErrorCallback & transmission is failing. Pls help us.

This error callback function is not getting called when we connect to PC. But we are getting during modem (UART based)communication only. Whats purpose of this callback ? Is there any configuration need to add ?

PBira.1 by Associate II
  • 9526 Views
  • 25 replies
  • 0 kudos

STM32L4R9I Fast Program issue

I referenced the example from STM32CubeL4-master and run the Flash_FastProgram example, but when I execute to this line *dest_addr = *src_addr in FLASH_Program_Fast(uint32_t Address, uint32_t DataAddress), it will go to HardFault Handler, have any id...

YNeng.1 by Associate
  • 1366 Views
  • 3 replies
  • 0 kudos

SDCARD +DMA Writing issue

HiI have setup SDMMC1 over DMA2 channel 14 (Tx) and having issue in writing more frequent data. I have interrupt on system tick (pend sv) 1ms. When I write every 10ms 128 Bytes, it gives me ring buffer overflow error. That means it stuck somewhere on...

APate.8 by Associate II
  • 1230 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F207 CAN2 bootloader

in datasheet :Boot modes At startup, boot pins are used to select one out of three boot options:  Boot from user Flash memory  Boot from system memory  Boot from embedded SRAM The boot loader is located in system memory. It is used to reprogram th...

LUrba.1 by Associate II
  • 3903 Views
  • 6 replies
  • 0 kudos