STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem sending data concurrently via Composite USB

Hello there,I've setup a composite device (HID + CDC) on STM32F401RCT MCU. However, when sending data via CDC, the PC can only receive some HID packets (kind of lag issue) or no packet at all. I need to send data via HID and CDC concurrently. Is it ...

NChin.2 by Associate II
  • 1751 Views
  • 3 replies
  • 0 kudos

Can't ping STM32H743 with LwIP and FreeRTOS

Hi,SETUPI am currently working on an STM32H743XIHx integrated in a custom board. I am using the FW package STM32Cube_FW_H7_V1.8.0 and STM32CubeIDE V1.5.1 with STM32CubeMX V6.1.1.Software side, I am using LwIP and FreeRTOS middlewares, with a static I...

PBOGR.1 by Associate
  • 2740 Views
  • 2 replies
  • 0 kudos

H7 UDP example

Hello,We run on platform STM32H743ZI and I made new UdpEchoClient application using source STM32H743ZI _EVAL\Applications\LwIP (in other word UdpEchoClient for Nucleo144) without RTOS!Unfortunately , it doesn't work ...Maybe you know about any workin...

APasi by Associate II
  • 8426 Views
  • 18 replies
  • 0 kudos

Resolved! STM32F407 failed with printf float

Hello,I'm trying to setup the system based on SMT32F407 with ThreadX, and enable the print float option for logging feature. Everything works fine!But when we started stability test, thousands of logs are composed with vsnprintf, but it finally fails...

0693W000008yZcHQAU.png
XLei.1 by Associate II
  • 2071 Views
  • 2 replies
  • 0 kudos