STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

P-L496G-CELL02: Unable to setup eSIM

Hello,I am currently trying to run the X-CUBE-CELLULAR demonstration project as per the Getting Started Guide (UM2567). and "How to enable SIM MFF2 connectivity with P-L496G-CELL02.txt"I've have been unable to retrieve the BIC from the BG96 with the ...

AGiml by Associate
  • 759 Views
  • 0 replies
  • 0 kudos

both of stm32h743's usb host support dma?

hiOn stm32h743, usb hs1 with external phy works perfectly well in dma mode. Its perfoamance and reliability is very good.But usb hs2 with internal phy not work in dma mode. If I disabled dma mode, it works but not reliable. It's internl fifo sometime...

shark by Senior
  • 1344 Views
  • 1 replies
  • 0 kudos

AzureRTOS for STM32H753ZI poor code quality

Hi,I tried to make a Azure RTOS ThreadX project but i saw very poor code quality which makes me unsure if I made the right decision.In the file tx_api.h there are alot of for example following declaration:#define tx_thread_create(t,n,e,i,s,l,p,r,c,a)...

Osto by Senior
  • 3041 Views
  • 6 replies
  • 0 kudos

Possible to use USB in STM32G0B0KE (32pin)?

In datasheet STM32G0B0KE/CE/RE/VE, DS13565 Rev 2, page 28/105 this can be read:"The embedded USB controller cannot be used on STM32G0B0KE as this device does not provide an HSE oscillator input."As it is written on same page "the clock source must us...