2020-06-17 1:19 AM
Hi Folks,
Need a bit help in trying to figure out what's going on.
I have been trying to port the
en.stm32cubeg4_v1-2-0\STM32Cube_FW_G4_V1.2.0\Projects\B-G474E-DPOW1\Examples\FMAC
FMAC_Buck_VoltageMode_HW_AN5305
to a
NUCLEO-G474RE platform.
I am trying to observe HRTIM TC1. TC2 waveforms on the NUCLEO-G474RE board.
AFAICS, the difference between the NUCLEO-G474RE and the B-G474E-DPOW1 is the lack of a Joystick and the MOSFET's. Is the example a fully working example, any thoughts ?
(Maybe it has some issue to run on the NUCLEO board, ..)
I wondered at least I could monitor the waveforms on the NUCLEO board. but the example does not seem to run/generate any waveforms.
Kind of clueless, digging through the HAL code as to why the example wouldn't generate the HRTIM waveform on the NUCLEO board.
Is there something that i am missing ?
Thanks,
Manu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.