STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about speex

Hello everybodyI want to use speex in my project based on st application note in speex demonstration and it's code ... my hardware is f407 discoveryMy question is : is there any option to implement speex in wideband mode with good quality in f407 boa...

ARSL.1 by Associate
  • 966 Views
  • 0 replies
  • 0 kudos

HTTP IAP and Google Chrome

Hello,I worked on a web server based on a Nucleo STM32F767ZI card and also on remote reprogramming with HTTP. For remote reprogramming I used an example (https://www.st.com/en/embedded-software/stsw-stm32069.html) which I adapted myself.Unfortunately...

SBebi.1 by Associate II
  • 1524 Views
  • 1 replies
  • 0 kudos

VCP ISSUES

I am having VCP issues in Windows 10. I have seen similar threads regarding similar behavior but have not found, or seen, any definitive solutions.STM32 driver download page states :" Starting from Windows® 10, the STSW-STM32102 driver is no more ade...

AKluk.1 by Associate II
  • 3736 Views
  • 9 replies
  • 0 kudos

[STM32F411] I want UART waiting for RXNE interrupt,but it can't stop to keep entering UART_IRQ_Handler and alway readed the last data even I'm not trans any data to MCU, Where am I doing wrong?

UART_HandleTypeDef huart2;void MX_USART2_UART_Init(void){ huart2.Instance = USART2; huart2.Init.BaudRate = 9600; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.M...

WYang.5 by Associate
  • 1432 Views
  • 1 replies
  • 0 kudos

How to establish cellular MQTT with P-L496-CELL2 ?

Hi, I recently acquired P-L496G-CELL02 development kit to establish cellular communication with MQTT (own server). Firstly, I could not get the BIC value while following the steps as shown in the "How to enable SIM MFF2 connectivity with P-L496G-CELL...

FHATI.1 by Associate
  • 1167 Views
  • 0 replies
  • 1 kudos

Resolved! STM32F4 USB Device Custom HID example

I am using a custom board with STM32F4 micro and I want to use the Cube libraries. I need a simple example of application of a USB Device configured as Custom HID. I need to know not only how to configure the USB, but also how to transmit data to the...

VCapu by Associate III
  • 6542 Views
  • 10 replies
  • 0 kudos