STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L462 With USB DFU goes into Hardware fault when in the methods from usb_dfu_if.c I use the HAL_FLASHEx_Erase.

I have made a DFU application on the STM32L462RET6 CPU.From the CUBEIDE I set the:HSEEnable USBSelect the DFU as a Class For fs Ip.Set the app start address to 0x8008000 Set the DFU media interface to @Internal Flash  /0x08000000/01*032Ka,01*480KgSet...

MRosc.1 by Associate II
  • 1612 Views
  • 3 replies
  • 0 kudos

Resolved! Stm32CubeF4 I2C examples for different boards

Hi,​Im trying to establish an I2C communication between stm32f446nucleo board and stl32f469i disco board,​​I flashed the stm32f446-nucleo I2C master code example from cubeF4stm32f446 into an stm32f446 nucleo board and the slave I2C code example from ...