STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7使用内部ram驱动4.3寸TFT彩�?时�?�到的内存问题

1.你好.请问我使用STM32H743ZIT6使用内部512Kram作为TFT彩�?的GRAM,�?�时还需�?使用USB HOST和文件系统.这�?方案�?�行�?�?​2.我的GRAM放在了512KB的RAM中,程�?�?行的RAM放在了128KB的DTCM中.但是打开内存管�?��?�编译器报错内存冲�?..�?�?�我在内存管�?�中删掉了几个内存池�?�显示工作正常.3.显示工作正常�?�,我�?�现使用内存管�?�为FATFS文件系统申请内存时出错,无法申请.请问这是什么原因呢?

心王.1 by Associate
  • 667 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F767 MQTT USING LWIP

I am new to LWIP and MQTT. I am trying to use MQTT using LWIP in stm32f767 . I am able to get ethernet connection up and ping also works. I use mqtt_client_connect to connect to the server. The function is as follows:-mqtt_client_connect(mqtt_clien...

sne_123 by Associate III
  • 14361 Views
  • 20 replies
  • 1 kudos

SDMMC, FATFS AND FREERTOS

I am working on FATFS, SDMMC WITH FREERTOS on NUCLEOH743ZI2. I use STM32CUBEMAX to config the program. however, the program doesn't work properly. sometimes, I can mount sd card properly, but when I try to open file. the program always get failed res...

yang hong by Associate III
  • 4902 Views
  • 7 replies
  • 0 kudos

STM32F401 HAL_FLASH_Program not working

Hi community.. I have the following code : bool FLASH_WriteDoubleWord(uint32_t flashAddress, uint64_t Data) {   FLASH_Unlock(); /*clear some flag*/ __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR ...

SGasp.1 by Senior
  • 4586 Views
  • 14 replies
  • 0 kudos

Resolved! AzureRTOS - tips/guides for getting started

Hello,I am trying to start a project with AzureRTOS with the STM32H723 Nucleo board and am looking for some tips, getting started guides, etc.I have looked at the Fx_NoR_Write_Read_File example project and saw how _tx_initialize_kernel_enter() was s...

MButsch by Associate III
  • 2991 Views
  • 5 replies
  • 0 kudos