STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem using µSD card with SDIO and FatFs

 I'm trying to make a program one of the features of which is SD card support. I'm using HAL libraries entirely, it's hard to find an example that combines SD card, SDIO communication and HAL libraries.1. problem is that function f_mkdir, f_open retu...

KMach.2 by Associate II
  • 8531 Views
  • 13 replies
  • 0 kudos

Resolved! STM32F4 USB composite device driver MISSING!

Hi!I currently work on USB composite device (CDC + MSC). I putted together a program with help from:https://sudonull.com/post/68144-CDC-MSC-USB-Composite-Device-on-STM32-HALhttps://www.programmersought.com/article/18127793400/The thing is, i don't kn...

bmak by Senior
  • 7570 Views
  • 7 replies
  • 0 kudos

BUG found on HAL STM32L4 HAL_UARTEx_ReceiveToIdle_IT(). This function works on STM32F0 HAL V1.11.3 but not on STM32L4 V1.17 An update is needed to solve bug when UART bytes is equaly to RxXferSize, because currently it stays on endless IT loop

A simple compare between the two HAL Versions shows that line 4730 "huart->ReceptionType = HAL_UART_RECEPTION_STANDARD" needs to be moved at position line 4708. This fixes the bug, same as it is implemented in HAL For STM32F0 series

VPapa by Associate
  • 1147 Views
  • 1 replies
  • 1 kudos