STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot from flash bank 2 broken on STM32G483VE

This is the same problem described in this thread, except the proposed solution does not fix the issue: https://community.st.com/s/question/0D50X0000CEqc1SSQR/dual-boot-on-the-stm32g4-not-quite-working-boot-from-second-bank-fails?t=1591957302322Basic...

TDani.2 by Associate II
  • 788 Views
  • 0 replies
  • 0 kudos

ADC DMA continuous mode stops FreeRTOS task.

Hi,I am using STM32F746 discovery board. I enabled FreeRTOS task and it is running fine. After I start ADC DMA function by enabling DMA continuous request mode and calling HAL_ADC_Start_DMA(), the RTOS task stops running. The ADC conversion stops the...

JChen.24 by Associate III
  • 3741 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H735G-DK STLINK no STLINK USB enumeration.

Hi,I just bought STM32H735G-DK and USB is not working out of the box.I have put jumper on STLK but device is not getting detected on PC(LD6 red/green dim lit).There are no new devices in device manager when plugged in.Board is running original progra...

BKrak.1 by Associate II
  • 5653 Views
  • 12 replies
  • 0 kudos

Resolved! STM32H743 unreliable micro SD transfers

Hello all,I have worked through a number of issues with the SDMMC system and am currently stuck with not being able to reliably transfer from micro SD. I wrote test code to repeatedly read a file from the external card. In some cases HAL_SD_ErrorCall...

AHigg by Associate II
  • 10536 Views
  • 19 replies
  • 1 kudos

STM32 Bootloader over USART with pin swapping

Hello All,Using STM32H743, I designed a board to use USART1 as the debug interface so that I could also bootload to this port. I am using an FTDI chip to create a virtual COM port. The problem is that I swapped the TX/RX pins in the design and had to...

JMill.1 by Associate III
  • 2637 Views
  • 4 replies
  • 0 kudos

STM32F072 can't work if doesn't connect the USB

Hi advancedI have a question to ask everyone. I use STM32F072 and use VCP to communicate with the GUI on the PC side.But it is very strange. If STM32F072 is not connected to USB, it will not work. It seems to be stuck and did not continue to execute ...

0693W00000HppUbQAJ.png 0693W00000HppUDQAZ.png
Simon.Lee by Associate II
  • 2160 Views
  • 5 replies
  • 0 kudos