STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Bootloader over USART with pin swapping

Hello All,Using STM32H743, I designed a board to use USART1 as the debug interface so that I could also bootload to this port. I am using an FTDI chip to create a virtual COM port. The problem is that I swapped the TX/RX pins in the design and had to...

JMill.1 by Associate III
  • 2639 Views
  • 4 replies
  • 0 kudos

STM32F072 can't work if doesn't connect the USB

Hi advancedI have a question to ask everyone. I use STM32F072 and use VCP to communicate with the GUI on the PC side.But it is very strange. If STM32F072 is not connected to USB, it will not work. It seems to be stuck and did not continue to execute ...

0693W00000HppUbQAJ.png 0693W00000HppUDQAZ.png
Simon.Lee by Associate II
  • 2163 Views
  • 5 replies
  • 0 kudos

LWIP -SRAM Ping Issue

Hi,I am working STM3240G-Eval Board. Integrated LWIP and able to ping without any issues. Followed the FSMC_SRAM_DataMemory example to change the data memory sram and I am able to allocate variable in SRAM. Now the issue is not able to ping. Please h...

HPras.3 by Associate
  • 1114 Views
  • 1 replies
  • 0 kudos

Resolved! debugger stops after HAL_TIM_Base_Start_IT .

Created a new STM32 project for STM32G030K8 without modifications, when i run the debugger debugger stops working after HAL_TIM_Base_Start_IT..I have selected TIM14 as timebase source as i'm using RTOS.Why does the debugger stops in a new STM32 cube ...

0693W00000Hpsy1QAB.png 0693W00000Hpt1sQAB.png 0693W00000Hpt1nQAB.png 0693W00000Hpt1iQAB.png
sde c.1 by Senior II
  • 2784 Views
  • 2 replies
  • 0 kudos

How to abort HAL_I2C_Slave_Transmit_IT

HAL_I2C_Master_Transmit_IT can be aborted via HAL_I2C_Master_Abort_IT.But how to abort HAL_I2C_Slave_Transmit_IT?There does not appear to be a corresponding abort function.If a callback complete does not occur, the software should be capable of abort...

A problem when receiving data with TCP LwIP

I had a problem when receiving data with TCP LwIP: Because TCP max segment size is 1460 so I can not receive the whole response from the server (2.75KB), I just received only 1440 Bytes. Are there any ways to receive full the response data? Can someo...

0693W00000GZ2oXQAT.png 0693W00000GZ2vDQAT.jpg
NLong.1 by Associate
  • 1770 Views
  • 1 replies
  • 0 kudos