STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429ZI Nucleo Ethernet Problem

Hi I am currently working on a project where I have to implement an Ethernet Driver. below is my code.I am trying to send ARP packets to my directly connected laptop without expecting response (Rx is not used). Code runs without MAC controller and DM...

LLOLO.1 by Associate II
  • 1103 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F407 + LwIP + DP83848 = Cannot Ping - Why?

I have an STM32F407 and I'm using LwIP + DP83848 Ethernet PHY. I'm facing problems to ping the unit and I don't know why.  The pinouts for the RMII settings. Red rings got to the processor. The blue ring shows RESET. It need to be logic 1 (HIGH) for ...

0693W00000LyBAkQAN.png 0693W00000LyBAzQAN.png 0693W00000LyBB4QAN.png 0693W00000LyBB9QAN.png
DMårt by Lead
  • 10407 Views
  • 7 replies
  • 0 kudos

STM32h7 AZURE RTOS USB FS CDC example is available?

Hello,I am working on NUCLEO-H745ziq board. The board support USB FS. I have to configure USB as CDC in AZURE RTOS . The example are provided for HS , so there is any example for FS CDC AZURE RTOS configuration. I am first time working on this AZURE...

MDeva.1 by Associate II
  • 1222 Views
  • 3 replies
  • 0 kudos

Programming one MCU from another MCU by UART or I2C

Hi,I have an STM32L552 MCU (the 1st) that has only two interfaces to the user, one through the USB-C and the other through Bluetooth. I have another STM32L031 MCU (the 2nd) inside the design that communicates with this L552 MCU through UART/I2C. Here...

ashah.16 by Associate II
  • 1659 Views
  • 1 replies
  • 0 kudos

Resolved! [SOLVED] STM32H7 SPI does not seem to work with DMA

Posted on March 07, 2018 at 13:01 EDIT: 14/03/2018 https://community.st.com/people/Schwaninger.Hannes‌ found that we need to use RAM_D1 and not DTCMRAM of the memory area. This is not made by default when we use STM32CubeMx to set SPI ...

0690X00000609ynQAA.png 0690X00000609w9QAA.png
Geo En by Associate III
  • 18607 Views
  • 29 replies
  • 0 kudos

Using UART bootloader on STM32G030J6

I am attempting to activate the bootloader mode on the STM32G050J6 (SO8N package). It is unclear to me from the documentation which pins are to be used. Currently, I am using pins 1 and 8 (USART1_RX and USART1_TX in the documentation respectively) as...

DBong.1 by Associate II
  • 8712 Views
  • 11 replies
  • 0 kudos