cancel
Showing results for 
Search instead for 
Did you mean: 

External Supply and USB Supply for STM32 F429ZI Nucleo. What is the difference between the schematic?

VKANT.1
Associate

We have a system that communicates with the engine controller via CAN communication on the STM32 F429ZI NUCLEO and has an APPS (Gas Pedal). When we supply this system via USB, the system works correctly, but when we supply the system with a 12V separate from the Vin leg, we cannot communicate with the motor driver. We can read the pedal with the LEDs on it, but it seems that there is a problem with CAN communication.

What is the schematic difference between USB supply and external supply? If there is a difference, what kind of system it can affect.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nikita91
Lead II

How does your CAN line driver is powered ?