STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing stm32f7 with USB 2.0 (pen drive)

Hello guys, in my project i want to store some sensor data to pen drive using stm32f7 dev kit so i have gone through some default code generation and i didn't get the configuration and also how to connect the pen drive to USB HS port i have following...

Pratyush by Associate II
  • 1155 Views
  • 0 replies
  • 0 kudos

Resolved! Extremely strange behavior running on an STM32G0B1

Ok, I'm at a complete loss here so I'm looking for any ideas or suggestions. We have a code base that runs on top of FreeRTOS and we have versions of the code that run on multiple, different STM32L4s and on the STM32H753. I ported the code base to ...

JKaz.1 by Associate III
  • 7238 Views
  • 13 replies
  • 0 kudos

Resolved! Integration guidelines for X-CUBE-CELLULAR and NETXDUO

Hi,I'm looking to port an application using the LwIP stack and X-CUBE-CELLULAR to NETXDUO. The goal is eventually create an application that connects to Azure IoT Hub over cellular.Are there any recommendations from ST on integrating NETXDUO with X-C...

MD'Si.1 by Associate III
  • 2041 Views
  • 3 replies
  • 2 kudos