STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is There a Way to Hack USB-PD on STM32G030K8?

Hi All, I designed my board with a STM32G0 series MCU with the main intention of using its USB-PD peripheral. I later realized that it is only the STM32G0x1 series MCUs would be capable of USB-PD while I will be receiving a board turn with an STM32G0...

NYou.1 by Associate II
  • 3170 Views
  • 4 replies
  • 0 kudos

Resolved! How to make SDIO_USB bridge using STM32F4 ?

Hi,I want to use STM32F4 to make an SDIO/USB bridge.I mean I want to send data received on SDIO interface to the USB otg interface and vice versa.I want to know if this is possible ? if yes, any implementation helpMany thanks,

YahyaYozo by Associate II
  • 2050 Views
  • 1 replies
  • 1 kudos

STM2Cube slow downloading

Hello,I have a problem with download speed updates of SW STM32CumbeMX and STM32CubeIDE and downloading packages. I find that I download it from 92.122.48.112:433orbut max speed is 160kB/s. Is there some settings to select server for actualization?Tha...

0693W00000QMLwdQAH.png
Pjesto by Associate
  • 1054 Views
  • 0 replies
  • 0 kudos

STM32 G071 System bootloader question

I am trying to use the system bootloader G071 MCU with NUCLEO board using USART2. The factory programmed flash option bytes are 0xFFFFFEAA, and after I modify the nBOOT0 bit the MCU resets and the bootloader is activated after setting FLASH->CR |= FL...

IPavl.3 by Associate
  • 1956 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F7 USB SOF and ID Disable/Reuse (Mbed)

I am trying to use the Mbed USBSerial class on an STM32F767VI and it works fine. I also have CAN3 RX setup on pin PA8 (USB SOF) and a GPIO on PA10 (USB ID). I am not using the SOF or ID functionality, but initializing the USB makes it so those pins d...

LLawr.1 by Associate II
  • 4863 Views
  • 4 replies
  • 0 kudos

I am trying to connect a STM32F417 to a Linux-host (RHEL 8 / CentOS 8) via FS-USB (USBX) as a CDC device under AzureRTOS(ThreadX) + USBX

I am trying to connect a STM32F417 to a Linux-host (RHEL 8 / CentOS 8) via FS-USB (USBX) as a CDC ( VCP ) device under AzureRTOS(ThreadX) + USBX. On the Linux host, it appears as '/dev/ttyACM0'.This results in the Linux host tries to send 'at' comman...

olebenny by Associate II
  • 802 Views
  • 0 replies
  • 0 kudos

zephyr support on NUCLEO_F439ZI board

Hi, I am using zephyr rtos for my application. I am running basic Blinky example on ST boards. I am able to build and flash that examples on nucleo_h743zi board. however same example am trying to run on nucleo_f439zi board. Here am getting "Invali...

Itachi by Associate
  • 2712 Views
  • 2 replies
  • 1 kudos

Lidar ethernet communication

Hi guys, my Lidar sensor named Livox Tele-15 communicates via ethernet. It gets IP by connecting to the modem in its own example application. It transfers data by connecting to IP in computer software. I want to control Lidar with a controller from S...

OKose.1 by Associate
  • 1653 Views
  • 1 replies
  • 0 kudos