STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-H723ZG + FreeRTOS + LWIP

Hello everybody. I'm trying to make LWIP work on NUCLEO-H723ZG board, but I can't even get a ping response so far, even with static (DHCP disabled) network configuration. The project uses FreeRTOS (CMSIS API v2) and is created with MX tool. It seems ...

rzingler by Associate
  • 133 Views
  • 2 replies
  • 0 kudos

USB Data Transfer with STM32L552E-EV

Greetings,Kindly, I would like to know which USB interface I can use to transfer data between the STM32L552E-EV and the reComputer J4012.I am working with TEE, and my goal is to send plaintext from the reComputer to the STM32L5 so that it can be encr...

Nirene by Associate II
  • 258 Views
  • 8 replies
  • 5 kudos

Resolved! Ethernet Lwip Ping

Hi, I want to set up the Ethernet peripheral of the STM32H743 microcontroller using lwIP, but I’m facing a problem and I can’t get a ping response. I have reviewed some codes, but they don’t fully explain the cause of the issue. Does anyone have expe...

Serial communication limited to 512 bytes

Hello, I am using a NUCLEO-H7A3ZI-Q to send and receive packets over serial. I have a varying payload size, so I am using: HAL_UARTEx_ReceiveToIdle_DMA(&huart3, rx_buffer, 4096); as this searches for an idle at the end of the frame to begin processin...

Pincate by Associate II
  • 214 Views
  • 7 replies
  • 4 kudos