Skip to main content
sabari1
Associate III
June 30, 2025
Question

Netx HTTPS POST request

  • June 30, 2025
  • 1 reply
  • 495 views

hi 

i am working with HTTPS client code on stm32u585 microcontroller, using netx tcp/ip stack for the implementation. my requirement is to create a HTTPS post request with a json payload( nearly 8000 bytes). is there any reference or example available on HTTPS post request using netx. all i can see is the get request in the official GitHub.

if any example or reference regarding this issue will be much helpful for implementation.

 

with regards 

sabarinath 

1 reply

mbarg.1
Senior III
July 1, 2025

HTTP messages are decoded in _nx_web_http_server_receive_data.c

Here GET and POST messages are selected

in case of POST, VOID _nx_web_http_server_put_process(NX_WEB_HTTP_SERVER *server_ptr, NX_PACKET *packet_ptr) is called 

inside _nx_web_http_server_put_process() nx_web_http_server_request_notify() is called

You have to provide nx_web_http_server_request_notify() and assignto your HTTP server in  nx_web_http_server_create()

/* Call the user supplied function to notify the user of the put request. */

status = (server_ptr -> nx_web_http_server_request_notify)(server_ptr, NX_WEB_HTTP_SERVER_PUT_REQUEST, server_ptr -> nx_web_http_server_request_resource, packet_ptr);

 

 

Andrew Neil
Super User
July 1, 2025

@mbarg.1 wrote:

HTTP messages are decoded in _nx_web_http_server_receive_data.c


That's the server side; I think @sabari1 is asking for the client side - ie how to make the request ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mbarg.1
Senior III
July 1, 2025

OOPS ..

@Andrew Neil is right.

As far as I know, no examples for this case.

I guess @sabari1 has to use TCP socket to send a packet with HTTP/HTTPS PUT request writing ad hoc code.

Later will have to manage server reply ...