User Activity

Hi,I was able to run a demo project on a STM32H573 dev board. I am using ThreadX and NetxDuo, with mqtt addon.I was able to connect to the mqtt broker and send/receive messages.I want also to be able to use the bsd sockets to send packets on layer 2....
Hi,I have a STM32F407G-DISC1 board. The final goal is to write a program that get data from the hardware and publish via mqtt, and via the usb (HID client). Also an integrated http server would be great.Is it there online an implementation example fo...