STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unwanted interrupts for EthernetMAC (MMC)

We use a STM32F746 with Ethernet (ETH). We found a possible problem of the using the Ethernet (ETH) with actived interrupt. The Ethernet (ETH) has one interrupt vector for all interrupts of the Ethernet (ETH) (e. g. Receive, or Early Receive, ...) A ...

DFU and USART on USB

Sorry about the dumb question.Is it possible to have DFU and USART on the same USB port on a custom board?I just want to upload firmware via USB and have the ability to receive sensor data output via UART using a virtual com port.Two different things...

Manny12 by Associate III
  • 3263 Views
  • 6 replies
  • 0 kudos

Firmware update over uart I/O pin config

Hello togetherActual I use the systembootloader to update the device over uart.Is there a way to reconfigure the unused I/O pin for the system bootloader? Or must this be done via a self-written bootloader?The problem is that some I/O pins take on a ...

42bytes by Associate
  • 1272 Views
  • 1 replies
  • 0 kudos

Hi all, I enabled USB on 407 controller in MS Class and through program I am enabling (MX_USB_DEVICE_Init();) and disabling (MX_USB_DEVICE_DeInit ();) it. Once enabled, it looks as though the controller gets stuck in a loop. It does not execute

other functions and just hangs. I am suspecting some interrupt flag not being cleared. Strangely it works on my laptop but not on a PC. An earlier version is working without getting stuck and shows SD card content. Any suggestions please?