STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Since STM32Cube_FW_F7_V1.17.0 the HAL I2C Functions do not work the same. For a huge project that used to work with no issues on STM32Cube_FW_F7_V1.16.2 the I2C Data line goes low and the Firmware reports an HAL_I2C_ERROR_SIZE. Is there a known bug?

We are using a STM32F76ZI for a consumer device.The Firmware used to work fine with no errors.Since STM32Cube_FW_F7_V1.17.0 the I2C communication does not work all the time reporting random I2C Errors. The most common error is HAL_I2C_ERROR_SIZE that...

lwIP / TCP tx'd pbuf ACK'd?

Hello,I have to admit that this is more a question concerning lwIP, but as I'm using a STM32F7...And the search engines haven't helped yet.I need to transmit TCP packets quickly, without waiting for TCP's ACK.Payload for these packets come from an ar...

LCE by Principal II
  • 6569 Views
  • 13 replies
  • 1 kudos

Since STM32Cube_FW_F7_V1.17.0 the HAL I2C Functions do not work the same. For a huge project that used to work with no issues on STM32Cube_FW_F7_V1.16.2 the I2C Data line goes low and the Firmware reports an HAL_I2C_ERROR_SIZE. Is there a known bug?

We are using a STM32F76ZI for a consumer device.The Firmware used to work fine with no errors.Since STM32Cube_FW_F7_V1.17.0 the I2C communication does not work all the time reporting random I2C Errors. The most common error is HAL_I2C_ERROR_SIZE that...