cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-LPM01A PowerShield - Dynamic Current Range Too Limited?

Andrew Neil
Super User

The X-NUCLEO-LPM01A PowerShield has a dynamic current range maximum of only 50mA.

This is a long way short of the maximum current found in many STM32 applications; eg.

  • STM32WL - max Tx current is 120mA;
  • B-L072Z-LRWAN1 - max Tx current of the radio module is 128mA

Particularly annoying is that the PowerShield will simply abort the acquisition when the 50mA limit is exceed; eg, see:

https://community.st.com/s/question/0D53W00000KpzoVSAR/stm32l562edk-current-up-to-150ma

and:

https://community.st.com/s/question/0D53W00000ku5QLSAY/stm32cubemonpower-unhelpful-error-message-released-due-to-connection-issue

This makes the PowerShield useless in these applications.

Is there any workaround to this?

Even if it just gave an 'out-of-range' value in the logs, that would be preferable - then we could get measurements for all except the peaks using the PowerShield, and only have to find other means to measure the peaks.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
Richard.Chvr
ST Employee

Hi @Andrew Neil​ ,

As mentioned in https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-performance-and-debuggers/stm32cubemonpwr.html, ST offers currently 2 solutions that allow users to monitor current.

  • From 100 nA up to 50 mA with ~2% accuracy for the X-NUCLEO-LPM01A expansion board
  • From 300 nA up to 150 mA with ~2% accuracy for the Energy Meter of the STM32L562E-DK Discovery kit

Also I think that the STM32L562E-DK Discovery kit could be the appropriate solution for your needs.

https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-mpu-eval-tools/stm32-mcu-mpu-eval-tools/stm32-discovery-kits/stm32l562e-dk.html

              Moreover a new solution with a highest max current value is currently under development. Due to business reasons we can’t communicate about future availability of this new product.

Regards

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Ah - thanks for that. Worth a look ...

And looking forward to the new product ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

At the time of starting this thread, the STM32-LPM01-XN firmware for the X-NUCLEO-LPM01A board was at v1.0.1.

I see that the STM32-LPM01-XN firmware for the X-NUCLEO-LPM01A board is now at v1.0.6.

But I can't see any Release Notes.

Has anything been done about the behaviour on overload?

Again:

"Even if it just gave an 'out-of-range' value in the logs, that would be preferable - then we could get measurements for all except the peaks using the PowerShield, and only have to find other means to measure the peaks."

 EDIT

Asked as a separate question:

https://community.st.com/s/question/0D53W000014w80YSAQ/where-are-release-notes-for-the-stm32lpm01xn-firmware

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi Richard,

where can I download the PowerShield firmware for the STM32L562E-DK?

Did not find anything on www.st.com.

Thanks,

Wolfgang

@c_dev05​ "where can I download the PowerShield firmware for the STM32L562E-DK?"

EDIT: Just realised that I misread, and the following is all about the Host software - not the board firmware. :tired_face:

It should be on the 'Tools & Software' tab of the STM32L562E-DK Product Page:

0693W00000FCB44QAH.pngBut, indeed, it isn't:

0693W00000FCB77QAH.png 

But you can find it via the X-NUCLEO-LPM01A (the subject of this thread) Product Page:

0693W00000FCB9IQAX.pngOr just search for "STM32CubeMonPwr" or "STM32 Cube Power Monitor"

0693W00000FCBC2QAP.pnghttps://www.st.com/en/development-tools/stm32cubemonpwr.html

@Richard.Chvr​ - so why is it not linked from the STM32L562E-DK Product Page ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi Andrew, You're right. We just asked to our marketing responsible to update the STM32L562E-DK product page with a link to the powershield Firmware.

Thanks & Regards

@PDEFO.1​ I Just realised that I misread @c_dev05​'s post, and all I wrote in my previous post was about the Host software - but @c_dev05​ wanted the board firmware. :tired_face:

I also can't see the board firmware on the product page - do you know where that is?

EDIT

I guess that's covered under 'Demonstration software' in the Data Brief?

0693W00000FCCjHQAX.png

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hello,

this is correct. I was looking for the Board firmware.

Today I received the board and there is a firmware for current measurement v1.0.6 installed. If there is no newer version, this is OK.

I want to use this board to measure the current for my own developed PCBA. There is a connector CN20 that can be used for this purpose as written in the schematic for the board:

  • Output connector to supply and measure external target:
  • PIN 1: GND
  • PIN 2: Voltage source, current is not measured, it is not a copy of ourput voltage
  • PIN 3: Output with current measurement
  • PIN 4: Output voltage copy with 150R protection serial resistor, current is not measured

But I can measure no voltage on Pin 3?

Where can I find documentation how to configure the board for this purpose?

Thanks,

Wolfgang

That's really nothing to do with this thread - please start a new thread for the unrelated question.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.