STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

recvfrom() is not working on stm32H7B3I-DK.

How to resolve recvfrom() issue on STM32_Network_Library. I'm using stm32H7B3I-DK board.FreeRTOSSTM32_Network_LibraryES_WIFI (BSP) When I tested UDP socket, sendto() was working.But recvfrom() was not working, it was blocked for ES_WIFI_MAX_SO_TIMEOU...

IChoi.2 by Associate
  • 1035 Views
  • 0 replies
  • 0 kudos

Resolved! I'm looking for STM32G Series product.

Hello?​As title, I want to know product with USB, FD-CAN, 2~3 DAC, etc.Problem is USB and HCLK are bound(using external clock), so that upper limit is determined to be low.(48, 96, 144 MHz in maximum 170 MHz)​For that reason, to ask the question, is ...

LSung.1 by Associate III
  • 3183 Views
  • 7 replies
  • 0 kudos

Resolved! I2S No operation what so ever.

I have 2 I2S ports. I have a masterclock from an external source.My clock config is set for external 24.576Mhz I2S clock.I have set up I2S1 in half duplex slave mode for an ADC. It is receiving data in DMA.I have setup I2S2 in half duplex master mode...

PCamp.2 by Associate III
  • 2879 Views
  • 2 replies
  • 0 kudos

Cortex M0 Bootloader to application jump.

I'm working on Over the Air and I have three components.Bootloader in first two pages (using stm32f09x) and applicaiton and then second application.I'm unable to jump to application from bootloader for a specific reason.I have one linker script, gave...

Vmere.1 by Senior
  • 2769 Views
  • 1 replies
  • 0 kudos

Resolved! Why USB Virtual Com Device miss Empty Byte?

I have created project USB Virtual Com Device on STM 32F407. I set size of parcel = 32 byte. When i send parcel and befor parcel ends byte will be "0" STM 32 don't read bytes after "0". If no "0" byte always is OK. What doe's it mean? How get full pa...

0693W00000WItotQAD.png 0693W00000WItp3QAD.png
ABask.1 by Associate II
  • 2610 Views
  • 6 replies
  • 0 kudos