User Activity

Good morning everyone,I have an application where a STM32G474 as SPI master interacts with another ST controller as SPI slave. These are full-duplex DMA transfers of about 500 bytes at 10MBit transfer rate. The slave signals that it is alive via a di...
Hi guys,I have a problem with the internal temperature ADC-channel. I am trying to read a few analog values with ADC1. The ones I read from pins are perfectly fine but when I change the input voltage on PC13 (channel 13) this changes the value read o...
Hello all,I have a strange behavior with the ethernet connection of my STM32F207 application:When I flash the software to the controller the software works. I can ping the controller, I can communicate with a client software to the serversoftware on ...
Kudos given to