STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to properly configure DMA in order to use linked list in non secure Application (TZEN = 1) on STM32U585

Hi,our porject use TZEN =1;A custom Bootlaoder (secure app) is executed at begin and after we call a non secure Application.The non secure Application as already been tested/validated with TZEN = 0.This application use GPDAM channel 10 ro read data f...

0693W00000WL5hyQAD.png
Aurelien1 by Associate III
  • 1690 Views
  • 1 replies
  • 0 kudos

SD card SDIO 1bit is killing UART3

I am using STM32F103VGT chip and custom PCB with USB, graphics LCD (FSMC mode), RTC, CRC, ADC, TIM2, TIM4 and UART3 (DMA/IRQ).When I added SDIO, one data line (poling, IRQ or DMA) and FATFS, I noticed, that after mounting, reading and writing to SD c...

LLeva.1 by Associate III
  • 2224 Views
  • 4 replies
  • 0 kudos

Resolved! RM error: I2C Transfer figure wrong (RELOAD bit)

Hi,in RM STM32G4 (I use Rev. 7, page 1882, Figure 648 "Transfer sequence flow for I2C master transmitter for N>255bytes":The "RELOAD=0" info in last box at "N<256" is wrong.It must instead say RELOAD=1, AUTOEND=1 (otherwise Stop bit will fire immedia...

flyer31 by Senior
  • 2796 Views
  • 4 replies
  • 0 kudos

Flashing internal memory thru DFU Bootloader

Is it possible to flash the internal memory of a blank STM32L496ZG through USB? The device has Boot0 pulled down to GND, but all the memory banks are blank, from the application note it's unclear whether the MCU executes the embedded system bootloade...

gcastoldi by Associate II
  • 2769 Views
  • 5 replies
  • 0 kudos