Is there a register to set the outputpower on the ST25R3916 like on a Texas Instruments RFID transceiver? Or is the output power entierly controlled by the DPO?
Hello community!To whom it may interest:I made a RNDIS demo project and would like to share it with you.It is using HAL with my rndis library and FreeRTOS on top. Further I have implemented a lightweight http server, dns and dhcp server. The demo wor...
Hello,I'm searching for a yocto package which is using the USB DFU protocol in connection to a stm32 microntroller to do a fimrware update. Is there something around? Wasn't successfull on my search so far.BRNico
Hi,I have (for example) a byte array with the size of 6. Now I want to calculate its crc32 value. The first 4 bytes are no problem - I put them in as word, but what about the last 2 bytes?Thanks for the Help in advance.BRNico