cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in CubeMX with STM32H747 DualCore and AzureRTOS

AZorn.1
Associate III

Hello, maybe I found a bug in CubeMX.

Actually it is not possible for me to generate Code for the DualCore derivates to get AzureRTOS active on BOTH cores.

After activating a new project with AzureRTOS selected for both cores, all of the port-*.c and *.h files are removed after further changes in GUI with new code generation.

This bug is very annoying, because using dualCore Azure an each Core is not usable in fact.

bestRegards

Alexander

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

this issue is internally tracked and will be fixed in the coming STM32CubeMX version. So for the moment, you'll need to delete that file each time before regenerating the project.

Sorry for the inconvenience.

regards

Haithem.

View solution in original post

8 REPLIES 8
Haithem Rahmani
ST Employee

Hi @AZorn.1​ 

Which STM32CubeMX version are you using?

could you share a sample .ioc project that shows the issue.

AZorn.1
Associate III

Hello,

and thank you, for the fast response. Hopefully we can find a solution for this problem.

this is the first *.ioc directly after creating a new project.

AZorn.1
Associate III

*.ioc after activating threadX for M4 AND M7 both Ports are available in Project Explorer, everything seems ok so far.

AZorn.1
Associate III

*.ioc file after activating TIM1. Now the port-files for cortex_m4 are missing, the project is broken. Both Azure SoftwarePacks are still activated, but will not be exported correctly.

I am using STM32CubeIDE V1.7.0 with STM32CubeMX 6.3.0-RC5

best Regards

Haithem Rahmani
ST Employee

Hi,

Issue reproduced, could you try to remove the file '.mxproject' located under the root folder of your project then regenerate?

regards

Haithem.

AZorn.1
Associate III

Hello,

thank you for this hint, seems that, after deleting .mxproject both ports are generated correct. But only once, after changing anything else in cubeMX, the port is missing again.

Is it necessary to delete this file, prior to every code generation, to be sure, all code is generated correctly?

br

this issue is internally tracked and will be fixed in the coming STM32CubeMX version. So for the moment, you'll need to delete that file each time before regenerating the project.

Sorry for the inconvenience.

regards

Haithem.

AZorn.1
Associate III

Ok, thank you for the information and the support.