STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to send data over USB using Nucleo-L053R8 ?

Hi community, I am trying to use a Nucleo-L053R8 board to send data over USB without much success. The purpose of my project is simply to test the USB communication by sending string over USB Port as a first step before sending the sensor data. When ...

fakhfakh by Associate
  • 1766 Views
  • 1 replies
  • 0 kudos

Resolved! Verify if it is safe to continue I2C communication after I2C transaction instead of using HAL_Delay

I made an I2C communication between STM32U585 uC to an I2C EEPROM and it worksI do the following  but if I remove the HAL_Delay(10) or minimizes it to less than 10msec things are not working well, the second call I2C_Master_Transmit fails.Is there's ...

0693W00000aIwB7QAK.png
bmn by Associate II
  • 4522 Views
  • 8 replies
  • 0 kudos

how to enter the USB DFU mode in STM32L162VE?

Currently, I am using the STM32L162VE custom board. I want to enter the USB DFU mode but am not able to enter the mode. This chip supports the USB and USART pre-programmed bootloaders. I have referred to the application notes AN2606 and AN3156. I did...

0693W00000aIvUhQAK.png 0693W00000aIvVBQA0.png 0693W00000aIvVLQA0.png
VNasa.1 by Associate
  • 2429 Views
  • 3 replies
  • 0 kudos

Resolved! Mem/BusFault at internal memory regions (0xE0...)

Hello,I saw a not yet reproducable fault at adresses, which are part of the private/vendor-specific memory regions.The fault happend on a STM32H7B0 runnig freeRTOS, ICache + DCache enabled:Causing instruction address: 0x7.... (external flash)Comming ...

TNeub.1 by Associate III
  • 6297 Views
  • 10 replies
  • 0 kudos

Resolved! I have a USB problem with "nucleo_l476rg" in version RTOS V3.3.0 where my overlay works fine with RTOS V2.7.4 Overlay has been Migrated to the new way used in V3.3.0.

I have a USB problem with "nucleo_l476rg" in version RTOS V3.3.0 where my overlay works fine with RTOS V2.7.4Overlay has been Migrated to the new way used in V3.3.0.Error Message: Booting Zephyr OS build zephyr-v3.3.0 [00:00:00.000,000] <err> usb_dc_...

Tt.1 by Associate II
  • 3388 Views
  • 2 replies
  • 0 kudos