STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 Jump to (FDCAN) bootloader from the application - is the code we use for this purpose correct? is required also code for memory remapping?

We are not sure it really jumps to the bootloaderPlease see code attached, especially note if required to add code for memory remapping:void jump_to_bootloader(void) { void (*SysMemBootJump)(void);   /** * Step: Set system memory address. * *...

RLanz.2 by Associate III
  • 1914 Views
  • 2 replies
  • 0 kudos

Copyright for ST manuals, and reprinting excerpts

I'm writing a book about using FreeRTOS on an ST MCU.I'd like to use excerpts from the MCU reference-manual in the book, including figures.Surprisingly, the MCU reference-manual does not have an ST copyright.Are there any limitations or restrictions ...

JimYuill by Associate II
  • 1000 Views
  • 0 replies
  • 0 kudos

STM32H745 and Ethernet

I have read quite a few threads about ethernet on the H7, along with several internet posts. Part of me wonders if I should even try... But I am.I've followed this guide:https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethe...

0693W00000aJMqQQAW.png 0693W00000aJMqVQAW.png

task is not running after hard reset in freertos

hi,I make bootloader to switch the code between two bank starting at address 0x08000000.and two application starting at 0x08020000 and 0x08100000 respectively, when I individual run the code it work fine, but when I hard reset the code, it goes to bo...

ykn by Senior
  • 1141 Views
  • 0 replies
  • 0 kudos

How to fix the I2C slave issue with STM32G070? HAL_I2C_ListenCpltCallback, HAL_I2C_AddrCallback, HAL_I2C_SlaveRxCpltCallback, HAL_I2C_SlaveTxCpltCallback

Hi, I'm trying to setup a stm32g070kb (32pin) MCU as I2C slave by using CubeIDE.I would like to create a code which will work same as I2C Eeprom, but when I ask the stm32 (with another MCU) to return me a register or registers value, the returned reg...

0693W00000aJJ7hQAG.jpg 0693W00000aJJBPQA4.png
MrLKovacs by Associate II
  • 6983 Views
  • 8 replies
  • 0 kudos