STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 USBX Device and mount/eject SD card

Hi ST community// --- EDIT --- Missed preview and made some corrections / clarificationsI'm looking for a way to mount a SD card using the Azure RTOS UsbX MSC class, while the MCU is running. The code is mostly based on the ST examples, e.g.:https://...

DZimm.9 by Associate II
  • 385 Views
  • 2 replies
  • 1 kudos

Developing/Integrating AWS and MQTT Stacks

I have integrated lwip on my STM32H563RGT6  library and my requirement is to establish connection to my AWS endpoint from MCU to the cloud along with certificates. help me by providing the necessary stacks.Were my requirement is to send/publish some ...

aravindpv by Associate III
  • 291 Views
  • 1 replies
  • 1 kudos

USB HID Stm32f767

Hello, I've built a project with an STM32F767 and a USB HID connection. I also have a Visual Studio 2010 application to set PA0 to 1 for testing. My connection is established, and in Device Manager, the USB Custom HID device is recognized, but I can'...

PSEBA.1 by Associate II
  • 244 Views
  • 1 replies
  • 1 kudos

Resolved! Using USB-PD SRC and USB-CDC Device together

Hi @FBL I am working on a similar project like This one (USB CDC ACM device with Power Delivery in Source mode using USBX in standalone mode, FreeRTOS and USBPD with a TCPP02). The STM32 used is the H573I.I have found some code to add in the function...

Aristy by Associate II
  • 767 Views
  • 7 replies
  • 1 kudos

One Pulse Mode not working

My goal is to use timers to follow the required timing steps for a module I’m working with. To achieve this, I decided to use two timers — TIM1 and TIM2.TIM2 is responsible for counting the T1 time step. For this, I’m using One-Pulse Mode, so TIM2 is...

MichalPorazko_0-1762109266115.png MichalPorazko_2-1762110115913.png MichalPorazko_3-1762110191312.png

STM32F4 TIM6 initialization

Dear all,I'm working on a project based on STM32F479 and FreeRTOS. In this project the microcontroller is connected via I2C and SPI bus to other devices, such as switch ethernet and spi-uart converter. I run the initialization of these devices before...

MGall.11 by Associate III
  • 4320 Views
  • 12 replies
  • 1 kudos