STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 C011

Hi,I am going to be a part of a firmware development using STM32C0 series. Can I able to use ADC input which is input power supply as EXT Interrupt  to wake up from sleep mode?How can be it assigned in ?Please Can anyone give an idea?

meena by Associate III
  • 1680 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G070RBT6 I2C communication with ESP32 S3 C1 devkit

Hi, I am new to STM32, I am trying the i2c communication between stm32 and esp32. I am using STM32 as slave and ESP32 as Master. I am using Arduino IDEI connected stm32  PB6-SCL, PB7-SDA to esp32  GPIO21-SDA, GPIO19-SCL.i was not getting any response...

RamyaD by Associate II
  • 4788 Views
  • 3 replies
  • 1 kudos

Resolved! USB-C PD 3.1 support, when will it come?

Hi ST, we are looking for solutions to supply > 100W over the new USB-C PD 3.1 spec, but due to the (very) short time since the release it seems that no one has updated its specs yet.So I would like to know how and when is ST going to officially supp...

USB OTG_FS (device mode) CDC-ACM: IN endpoint freezes

We are working on radio dongle application using STM32F411/13. We have mostly everything working, except for a lingering issue with USB. Details of the issue are as below:The radio dongle application enumerates as a CDC-ACM device as expected.And we ...

MSuhe by Associate III
  • 1595 Views
  • 1 replies
  • 1 kudos

Programming the STM32G030F through serial interface

Greetings,I've always programmed MCU's using USB connector (e.g., on Nucleo boards) or through JTAG (for custom boards).  We are considering STM32G030Fx (TSSOP20 package) for sensor control - however, I need to figure out how to program the chip.  Fr...

RickH by Associate
  • 6605 Views
  • 1 replies
  • 1 kudos

LWIP and FreeRTOS using Nucleo-144 F429zi

Hi, I am using STM32f429zi nucleo-144 board to configure Ethernet using LWIP and FreeRTOS. But my program doesn't execute after "MX_LWIP_Init();" in the StartDefaultTask. What could be the issue? It halts on the below function inside queue.c.Function...

SSala.3 by Associate III
  • 2777 Views
  • 4 replies
  • 0 kudos