STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FD CAN STM32 in NORMAL MODE For STM32H745I-DISCO

Not sure this is the right label Is there  a link  where I can obtain the complete program code for STM32 FDCAN in NORMAL MODE for the STM32H745I-DISCO ( Tutorial ) similar to the entire code MULTI Can .zip  that was found i the link for the STM32 Ca...

MROWL by Associate III
  • 1471 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 ST-LINK Utility

Hello,I have a new PC Windows and and I have this error when I start the software STM32 ST-LINK Utility (file in attachment)It misses dll file (mfc140.dll)And idea please?ThanksArnaud 

Capture d’écran 2023-11-17 111619.png
Arnaud1 by Associate III
  • 8130 Views
  • 4 replies
  • 1 kudos

Firmware Update via USB-Stick

Hello Everyone,I hope you are well.I'm working with an STM32F401 microcontroller (Nucleo-F401RE) and my goal would be to update the firmware via a standard USB stick.Is this possible with the above controller? If so, can you give me  any examples? Th...

Eros2023 by Associate II
  • 12317 Views
  • 10 replies
  • 2 kudos

STM32F407VG

Hi Team,        I this microcontroller power consumption is 240mA.But we need much less than current consumption Specification ETHERNET,SPI,EMI,RTC.Pls give some  Low power consumption recommended IC List.And any Single core ARM CORTEX R Series avail...

Aravind by Associate III
  • 1448 Views
  • 1 replies
  • 0 kudos

RMII Mode link problem

I'm using STM32F407 and Marvel 88E6390X switch in our project. But we have some I2C problems so we added I2C recovery function using TIMER8. The ethernet ports doesn't work stable after this addition . When we removed the I2C function in the projec...

gabay.1 by Associate II
  • 3965 Views
  • 6 replies
  • 0 kudos

Resolved! I2C communication

Hello Everyone,I am using STM32F401CBU6 controller in my project and in this project it consists of 2 I2C slaves 1) Sensor 2) EEPROM.I2C1 is connected to slave and can able to communicate with the slave, later i have connected external EEPROM, starte...

Anil3 by Associate III
  • 9950 Views
  • 9 replies
  • 3 kudos