STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UART output is garbled on Tera Term

I ran the example project and successfully displayed “Hello World” on Tera Term.Then I tried to port this project into my own one.However, the result was garbled characters in the terminal.The baud rate (115200) and PLL/clock configuration are the sa...

chachamaru_0-1762764753839.png chachamaru_1-1762764754652.png chachamaru_2-1762764753839.png chachamaru_3-1762764753837.png

USB microphone from the USB speaker example

Hi,Tried to convert STM32CubeN6\Projects\STM32N6570-DK\Applications\USBX\Ux_Device_Audio_2.0 example of the USB speaker to the USB microphone on STM32N6570-DK.The USB device is enumerated as an audio recording device, ux_device_class_audio_stream_fra...

ERROR by Senior
  • 206 Views
  • 1 replies
  • 0 kudos

STM32N6: DMA2D is not working with AXISRAM3

Hi,I have a DMA2D issue with a STM32N6 Nucleo-144 board. I can use the DMA2D to blend two framebuffers if the inputs are in the AXISRAM1. However, when one of the framebuffers is in AXISRAM3 (NPU RAM), the DMA2D doesn't copy from the relevant framebu...

akosnagy by Associate
  • 294 Views
  • 0 replies
  • 0 kudos

STM32U5A9 and X-CUBE-AUDIO?

Hi,I'm getting info on playing mp3 files with my custom Nucleo-U5A9 (originally a NUcleo-U575, I replaced the MCU and added xtal). I'll be using the audio codec TLV320AIC3110 with I2C and SAI from the U5A9. I'll be using ThreadX, FileX an a uSD card....

Rodo by Senior
  • 325 Views
  • 3 replies
  • 1 kudos

Push Pull PWM

Hello ST, I am having some trouble generating two PWM signals for a push pull converter.  Ideally I would like the PWM outputs to look like this, I would like the PWM frequency to be 100kHz and a duty cycle range of 0% to 50%. I have connected the p...

allanoverst_0-1762377988597.png PWM PA0 and PA1.png