STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

My Pack Couldt add

Hello. i have installed my pack but it wasn't on the left side. (I-CUBE-RBUF)But other packs added before.https://github.com/nimaltd/STM32-PACK/but when i installed from local disk. it works.

nimaltd_0-1711489256164.png
nimaltd by Senior
  • 1342 Views
  • 4 replies
  • 0 kudos

Ram Function hard fault on return.

I have a STM32L476RG Nucleo-64, and I am trying to run code from ram, but whenever I do it, it makes it to the function but does not execute the code, and on return it hard faults. I am not trying to put all code in ram just one function. /* USER COD...

Module for Establishing PPP Communication and Integrating NetXDuo TCP/IP Stack in STM32 Projects

Hello everyone,I'm working on an STM32 project where I need to establish PPP (Point-to-Point Protocol) communication with a GSM module, such as the SIM7600. Additionally, I aim to integrate the NetXDuo TCP/IP stack into the project for network commun...

Resolved! ADC Read Maximizing Precision and Accuracy

Hello community,I'm looking for some feedback on how to optimize the ADC peripheral when using a handful of single-ended channels.I have an STM32H735G-DK and have 4 NTC3950 type thermistors connected to 4 of the Analog pins from the Arduino headers, ...

taylors by Associate II
  • 6451 Views
  • 5 replies
  • 0 kudos

Resolved! Bootloading from SD card STM32F4

I'm facing difficulties bootloading or upgrading firmware on an STM32F405 MCU from an SD card.Could anyone recommend a library or resource for achieving this? I've already tried a few methods but haven't had any success. Any help would be greatly app...

Resolved! Array for GPIO pins

Hello,   I am new to STM world. I am trying to make an array of GPIO pin in this format {{PIN1_GPIO_PORT, PIN1_PIN}..... This would then be used in custom function so I can dynamically access this pins. How should I declare such array and how would i...

Huzo by Associate III
  • 11561 Views
  • 16 replies
  • 4 kudos

Resolved! STM32U5xxx UART communication problems

I am using the STM32U5A9J-DK for a UART communication test, and I expect to display the content sent from the computer's Serial port on the screen (textArea).I'm using UART1, 115200 Baud rate, 8 data bits, 1 stop bits, and I've turned on the UART int...

Assembly code to launch an application

I got this assembly code (see below) in an ST example code on secure boot and  and I don't understand some lines :why do we have to push R1 five times in a row?why is LR set to 0xFFFFFFF9? That is causing a hard fault at runDoes anyone have better un...

HABIJ.1 by Associate III
  • 3172 Views
  • 2 replies
  • 0 kudos