STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash erase operation fail CMSIS STM32L4

Hello,I am trying to implement a flash erase function, which is based on the reference manual. I am using the STM32L476RG nucleo board. From there the instructions are: To erase a page (2 Kbyte), follow the procedure below: Check that no Flash memory...

Resolved! How to config SDIO with FATFS?

Hi all,I config the SDIO & FATFS by cubeMx for my STM32F429BI board.When I config the SDIO to SDIO_BUS_WIDE_1B, everything is work well; Even the generated MX_SDIO_SD_Init() is NOT calling the HAL_SD_Init() function. (Why don't need HAL_SD_Init() , i...

Junde by Senior III
  • 3180 Views
  • 2 replies
  • 1 kudos

PWM with external trigger

Hello Team,I have an STM32F469NIHX and I am trying to implement a use case where I want Timer8_ch1  to be a slave to an external signal that I apply on pin D2 (PG7), which is not a source of timer at all. Upon reading the DS, I understood that I cann...

Jansunil by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos

Resolved! TIM1 output compare mode on STM32G070

Hi All, I am trying to generate variable frequency using TIM1 on STM32G070. I use TIM1 in output compare mode and PC8 as an output for channel 1. Pre-scaler is set to 0 and ARR to divider for whatever frequency I want. When checking registers I see C...

vladov by Associate
  • 2376 Views
  • 2 replies
  • 2 kudos

osKernelStart faults to HardFault handler

Hi All I working on a data logger code.   It is basic at the moment.  1, set a an ISRTimmer for 1sec. 2, When ISR triggered set a read bit in Datalogger register i set up. 3, Next loop thru main i test Datalogger register, if set go to a function and...

DaveBy2 by Associate
  • 2125 Views
  • 1 replies
  • 0 kudos

X-CUBE-USB-AUDIO multifrequency.

Hi.In X-CUBE-USB-AUDIO, You wrote:1. Does it mean that playback and recording can work simultaneously, and at different sampling rates? For example, playback at 44,1k, and recording at 96k?2. Does it mean that playback and recording may by governed b...

X-CUBE-UAC2.jpg

HAL_GetUID functions do not seem to work

The HAL_GetUID functions return the same value on different chips of the same series. I am using an STM32L0 series chip. This is my code:uint32_t serialw0 = HAL_GetUIDw0(); uint32_t serialw1 = HAL_GetUIDw1(); uint32_t serialw2 = HAL_GetUIDw2();Whic...